Jersey Water cuts operating expenditure and lab time
Ceramic filter improves reliability of ammonia measurement
Jersey Water is the oldest established company on Jersey. One small well in the parish of St Lawrence was the source of the first mains water ever made available to islanders. Now Jersey Water operates from 20 sites across the island and supplies treated mains water to over 90% of the population. The company constantly strives to meet the challenges of a rapidly expanding island population with limited natural water reserves – nearly all of the island’s water supply is derived from rainfall.
Clear benefits
As well as improving reliability, the solution has cut operating expenditure and reduced the maintenance effort.
Jersey Water achieved consistent and accurate results.
Two-stage water treatment
All water supplied by Jersey Water is treated at one of two treatment works at Handois and Augrès. The Handois works is supplied directly from the adjacent storage reservoir, which acts as a collecting point for water pumped directly from other reservoirs and raw water sources. Both treatment works use a two-stage method of water treatment comprising chemically-assisted sedimentation and rapid gravity filtration followed by disinfection using chlorine and ammonia (chloramination) and UV.
Measuring ammonia levels
In February 2014, Jersey Water purchased two Stamolys CA71 chemical photometric analysers from Endress+Hauser to measure the levels of ammonia in the raw water and post filtration. This measurement not only checks if the raw water in the reservoir has been contaminated as a result of agriculture or pesticides but also determines the correct dosage of ammonia for the chloramination process.
In order to comply with regulations governing the supply of drinking water, the company needs to detect extremely low concentrations of ammonia – less than 50 parts per billion (ppb). "We decided on the Stamolys CA71 because it’s the only instrument on the market that has that lower-end range," confirms Ian Young, Electrical Engineer and Assistant Asset Manager at Jersey Water.
Inconsistent readings
The analysers were connected to the water company's own sample filtration system consisting of a cloth filter in a plastic housing. But the filters regularly became clogged with organic matter and had to be replaced at a cost of €30 each. More crucially, the readings from the analyser were inconsistent with the results produced from samples tested in Jersey Water's laboratory.
Calling in the experts
Analytical experts from Endress+Hauser were called in to assess the problem. The CA71 analysers were sent back to the production centre in Germany for testing and it was determined they were working perfectly. More tests were carried out on the process and it was discovered that algae growth in Stamolys CA71 ammonia analyser the filtration system was to blame: the algae were consuming some of the ammonia before it could be detected by the analysers.
Replacing the cloth filtration system
The solution was to replace the cloth filter with a new sample preparation system from Endress+Hauser, Liquiline System CAT820. This has a ceramic filter that filters samples to 0.1 micron, small enough to allow the dissolved ammonia through but keep other particulates out of the prepared sample. The ceramic filter was fitted inside a custom-built flowcell as the ceramic filter is usually suspended in open tanks to filter samples for analysis by the new Liquiline CA80 analysers.
A real problem-solver!
The team at Jersey Water were impressed with the way the problem was resolved. "It was sorted out quickly and our contact at Endress+Hauser was really helpful," explains Ian Young. "The new filter is a really good piece of kit – the results are now a lot more reliable and consistent down the lower-end range."
The Liquiline System CAT820 and its ceramic filter unit have been specifically designed for preparing samples for colorimetric measurements in the water & wastewater industries. Here sample preparation is absolutely critical to ensure accurate and repeatable measurements for dissolved ammonia and phosphate in particular, as these are regulated measured parameters in both industries.
-
Standard products
- Reliable, robust and low-maintenance
Technical excellence
Simplicity
-
Specialized products
- Designed for demanding applications
Technical excellence
Simplicity
Variable
| FLEX selections | Technical excellence | Simplicity |
|---|---|---|
Fundamental selection Meet your basic measurement needs |
Technical excellence
|
Simplicity
|
Lean selection Handle your core processes easily |
Technical excellence
|
Simplicity
|
Extended selection Optimize your processes with innovative technologies |
Technical excellence
|
Simplicity
|
Xpert selection Master your most challenging applications |
Technical excellence
|
Simplicity
Variable |